This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I am very new to this TI based platform development work.
I have a requirement to drive BLDC Maxon motor using BOOSTXL-DRV8323RH along with TMDSCNCD28035.
Do we have any sample/example code with this configuration.
regards
Ramjee
Hi Ramjee,
The BLDC team only has BOOSTXL-DRV8323RH supported with LAUNCXHL-F28027C and LAUNCXL-F28069M InstaSPIN-FOC via MotorWARE, and LAUNCHXL-F280049C and LAUNCHXL-F280025C using MotorControl SDK.
I'll forward this to the C2000 team to see if they have any resources for driving a BOOSTXL-DRV8323RH using 2803x family of C2000 MCUs.
Thanks,
Aaron
There is no example code for BOOSTXL-DRV8323RH with TMDSCNCD28035, and the TMDSCNCD28035 controlCard can't install on BOOSTXL-DRV8323RH board directly.
You can find the example code for BOOSTXL-DRV8323RH with the newer C2000 device like TMS320F280025C as below.
You may download and install the latest MotorControlSDK, which can support a set of hardware kits and control algorithms for BLDC/PMSM drive. The kits include LAUNCHXL-F280025C with BOOSTXL-DRV8323RS, or BOOSTXL-DRV8323RH, or DRV8353Rx-EVM, or BOOSTXL-3PHGANINV, or DRV8316REVM. The control algorithms include InstaSPIN or eSMO based Sensorless-FOC, and incremental encoder or hall sensor based sensored-FOC,and sensorless trapezoidal BLDC control with InstaSPIN-BLDC. The detailed introduction about the lab can be found in the lab user’s guide as the links below.
C2000WARE-MOTORCONTROL-SDK: https://www.ti.com/tool/C2000WARE-MOTORCONTROL-SDK
Universal Project and Lab User’s Guide: https://www.ti.com/lit/spruj26
Example lab project at the folder: C:\ti\c2000\C2000Ware_MotorControl_SDK_<version>\solutions\universal_motorcontrol_lab\f28002x
Or you can find the motor control example code for F28035 in controlSUITE as the link below, but you have to port these example code to support BOOSTXL-DRV8323RH with TMDSCNCD28035.
[FAQ]Getting Started with C2000 MCUs for Motor Control
https://e2e.ti.com/support/microcontrollers/c2000/f/171/t/855709