Hi Team,
We running one stepper motor in normal condition it is working fine, the NFAULT pin is pulled-up.
later we are following the below steps.
1. We are introducing the error manually by making it Open Load.
2. able to detect the OL - reading the status register values as SReg0=0x81, sreg1=0x00, SReg2=0x03.
3. Manually removing the open load error.
4. also clearing the fault with CLR_FLT bit in CR4, still we are reading the register values as --- SReg0=0x81, sreg1=0x00, SReg2=0x03.
Could you please confirm why the registers reading the fault even after clearing the CLR_FLT bit.
Thanks and Regards,
Lakshmi Teja