Hi team,
Here's an issue from the customer may need your help:
1) When driving a three-phase MOS tube, it was found that the device has a default current amplification factor of 10 V/V. The customer would like to know how to change the default scale to 80 V/V.
2) After power-up, the SPI writes a current-amplification multiplier to control register 2, and when driving the MOS tube, it is found that GVDD voltage drops from 10.7V to 8.5V for 0.8ms, and then GVDD returns to 10.7V. The current amplification multiplier returns to the default of 10 V/V. Is this a reset of the SPI registers due to GVDD?
Could you help check this case? Thanks.
Best Regards,
Cherry