Part Number: UCC2626
Hi,
We are using UCC2626PW motor control IC. While simulating thermal Analysis at 75°C, we are getting component temperature of 84°C which is closed to operating temperature of the IC which is 85°C. Does that mean if the temperature of IC is increased by 1°C, the IC may fail in operation. Or else I need to compare this temperature with Junction temperature which is 150°C.
Please help regarding this.
Regards,
Kumar