Other Parts Discussed in Thread: DRV8428E
Hi team,
my customer wants to use motor driver on monitor XY movement application,
would you help check if this is OK, especially the VCC ?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Overall it looks good. The inductor (L501) on VCC is unusual and we don't normally recommend it. The inductor can cause ringing when it interacts with the bulk capacitor. I recommend testing the design without the inductor first (add a 0-ohm resistor there or solder bridge), and then only add the inductor back in if you have issues.
I can't see how large the bulk capacitor (PC5C1) is, as long as it is >100uF it should be fine.
If they would be interested in features of a more modern driver such as integrated current sensing and current regulation they might want to look into the DRV8424E or DRV8428E.
Regards,
Jacob
Hi Jacob,
thanks for your feedback
but the 100uF bulk cap is closer to DC/DC than DRV8836, DRV8836 only have 10uF MLCC closer, could this be a problem?
BTW, I don't think they want higher price only for current sensing and regulation function,
, do you have any other solution that is 2 phase and more suitable than DRV8366,
cost competitive is needed
Hey Fred,
Location of the bulk capacitor shouldn't matter, as long as the power traces/planes are sufficiently large. Should be fine.
Fair enough! Looks like you found the best chip for that application then. The only cheaper option I see is the DRV8833C, and it is only PWM control not Phase/Enable/PWM.
Regards,
Jacob Thompson
Hi Jacob,
what can stepper motor driver benefit from current regulation function ?
DRV8428E has this function while DRV8836 doesn't.
Regards,
Fred
Hey Fred,
The current regulation function allows you to set a lower value of current for the motor when you don't need full motor current. This can reduce the amount of power used in a system and keep the stepper motor from getting too hot.
Further, the DRV8428E has integrated current sensing, meaning that you don't need an external shunt resistor to measure the current. This significantly reduces the footprint size of the system since you don't need a large resistor and simplifies design a bit.
This training on current regulation explains it pretty well: https://training.ti.com/current-regulation
And here's a note on Overcurrent Protection (OCP) vs Current Regulation
Regards,
Jacob Thompson
thanks Jacob,
aside from power consumption perspective,
I see there's a slow decay with current regulation function, does it help on resonance or audio noise for stepper motor ?
Hey Fred,
Slow Decay is likely to help with the motor noise, but it isn't guaranteed. Check out 3.3.1 Effects of Current Ripple and Decay Mode in this "How to Reduce Audible Noise in Stepper Motors" note. Slow decay can help, but it isn't as effective as mixed decay or Smart Tune Ripple Control is (which the DRV8428E has). Using microstepping also typically helps with noise, higher microstepping levels ( ex. 1/256) will be quieter than full-step or 1/2 step.
Cheers,
Jacob
Hi Jacob,
got it,
so microstepping and mix decay both helps audio noise ,right?
Hey Fred,
Yes, both help.
Looks like I forgot to link earlier: How to Reduce Audible Noise in Stepper Motors
Cheers,
Jacob Thompson