This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8844: nFault triggered when VM powering up

Part Number: DRV8844

Hi team,

My customer is using DRV8844 and facing a nFault triggered when VM powering up.

As shown below, Yellow: nFault Pin voltage, Green: VM voltage

And if we increase the VM rise speed, like 2ms, no nFault is triggered. But the VM slew rate can not be increased because of the inrush current.

Support need

1. Is it normal operation for this device?

2. Why nFault will be triggered with slow VM slew rate?

3. How to work around it?

Sincerely,

Jayden Li

  • Jayden,

    Until the device crosses the UVLO threshold, logic in the device is not fully active.  This can cause indeterminate state on nFAULT pin.  It should be ignored on power-up case.

    Regards,

    Ryan

  • Hi Ryan,

    But it is not acceptable in my customer's application. And as I mentioned, they noticed it depends on VM slew rate, and what they want to know is what slew rate will not trigger this weird fault and if this can be avoided by controlling the VM slew rate.

    Thanks!

    Jayden Li

  • Hi Ryan,

    They need to know the specific data, like which slew rate, how much time will cause this unexpected issue? Thanks! 

    Thanks!

    Jayden Li

  • Jayden,

    You said that the customer can't increase the slew rate, so why does in matter if they can't do anything about slew rate?

    We need to find another way.  What is the length of the low pulse?  I can't tell from scope capture.  Do they monitor it with software?  

    They can make a software change to filter it or it can be filtered in hardware with a capacitor.  

    Regards,

    Ryan

  • Hi Ryan,

    I am trying to convince my customer if they can change the slew rate, but they need to know what slew rate is a guaranteed value for avoiding this nFault trigger. And then they can evaluate if they will control slew rate within this value.

    Thanks!

    Jayden Li

  • Jayden,

    I am sorry, but I don't think there is a simple answer here.

    Can you share the schematic?  Are LGND/GND connected together and to ground plane?  What is the state of nSLEEP and nRESET?  

    Regards,

    Ryan

  • Hi Ryan,

    Due to the urgency, I reached you through WEBEX to close this asap. You can find my answer in WEBEX window.

    Thanks!

    Jayden Li

  • Jayden,

    I will wait for your reply here as I requested.  I would like to see nSLEEP/nRESET on same scope capture.

    Regards,

    Ryan