This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
In DRV8844 EVM, I remove R1, add 10K resistance pull-high to 24V at nFault pin.
But I only can get about 7.5V at nFault pin.
In DRV8844 datasheet, absolute maximum ratings table shows:
Digital pin voltage range: LGND - 0.5 to LGND + 7 (V) -> I connect LGND to GND
Base on this table, I can't get 24V nFault, right? but why?
Abby,
nFault is open-drain type signal, this means during normal condition (no faults) this pin will see the pull-up voltage. SO if you pull-up to 24V, it sees 24V at this pin during normal conditions which is way too high than absolute max 7Volt above GND.
This is not allowed and may damage the device.
Best Regards
Milan-Motor Application Team
Hi,
Thanks for your reply.
Although nFault is open-drain, because the damage issue, DRV8844 is desinged to limit the digital voltage under 7V?
In the other word, nFault pull-high voltage con not over 7V.
Is my understanding right?
Yes I think designer might have limited it to 7V to protect the FET.
but As i mentioned, since its beyond the device absolute max rating, continous operation is not allowed.
Best Regards
Milan-Motor Application Team