We are developing a module with several DRV8873SPWP drivers. At this time we are unable to buy these chips, but we acquired some pre-production samples PDRV8245SPWPQ1 for testing. While reading the datasheets I found some differences that may be important for either testing or final product.
1. In documentation for DRV8245 it is suggested to add capacitor to IPROPI pin (8.3.4.1 Over Current Protection). There is no such suggestion in DRV8873 documentation. Does this mean the capacitor will not be beneficial for DRV8873?
2. For low speed ADC it is necessary to have low-pass filter on IPROPI output. What is recommended solution, simply put a capacitor on Rsense, or add RC filter after Rsense?
3. If we use PH/EN mode and connect two IPROPI pins of DRV8873 to the same Rsense resistor, will the output voltage behave the same way as on DRV8245? Specifically, since one of the high side FETs is always active, does this mean we will always see motor current on the output regardless of specific state of PH and EN signals?
4. The DISABLE (DRV8873), DRVOFF (DRV8245) and nSCS pins are internally pulled to 5V VDD. However DRV8245 documentation says "Internal pull-up resistance to VDD (reverse current blocked) ", while DRV8873S simply says "Internal pullup to DVDD". Does this mean DRV8245 can be directly connected to MCU pins and DRV8873S requires some kind of overvoltage protection on the MCU?