This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605: DRV2605

Part Number: DRV2605

Hi there

I am looking at using the DRV2605 Haptic Driver to drive an ERM motor in an upcoming project. The ERM motor has an operating voltage between 2.7V and 5V and has a rated current of 60 mA.

I am unable to find any information on the maximum current that can be sourced/sunk at the OUT+ and OUT- pin of the DRV2605. Can you please advise? 

Thank you.