This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8844: Can drive battery operated motor?

Genius 13999 points
Part Number: DRV8844
Other Parts Discussed in Thread: DRV8873

Hi Experts,

Seeking your assistance on this query from Cx:

Can you please let me know whether DRV8844PWP can drive battery operated DC motor?

If yes, can we connect 6 motors to one driver with motor parallel connection.

Thank you.

Regards,
Archie A.

  • Archie,

    As long as the battery voltage is within the range of the voltage specifications in the datasheet, this is no problem.

    As long as the current required to drive 6 parallel motors is within the range of the current specification in the datasheet, also no problem.

    We have plenty of higher power options as well like the DRV8243/4/5 or DRV8873/74.

    Regards,

    Ryan

  • Hi Ryan,

    Thank you for the information.

    Is there any temperature concerns we need to consider while connecting 6 motors into single driver?
    Can you please share your inputs on this?
    Or is it better to connect only two DC motors to a single driver?

    Regards,
    Archie A.

  • Archie,

    You will need to provide more information on the current profile for each motor and see which driver would be able to provide the total current.

    Regards,

    Ryan