This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey team,
I assume the WSON inherently has a better thermal profile than the DRL due to the thermal pad on the bottom to assist in removing heat?
Thanks,
Cam
But it has higher Junction to Board resistance (assuming includes the thermal solder pad under the case) of 42.6 vs 25.8, then how is the WSON better?
Also, it has higher junction to case (top) but has lower junction to ambient. How is this possible?
Brian
Is the Rja higher for DRL since the pins are directly exposed to the ambient environment? Ie the Rjb / Rjc being higher will result in more heat being moved off of the device to the board and the box heating up more than the ambient environment in comparison to the DRL, right Ryan Kehr?
Cameron,
There is a good app note that describes how all these measurements are done.
https://www.ti.com/lit/an/spra953c/spra953c.pdf
https://www.ti.com/lit/an/slma002h/slma002h.pdf - PowerPad specific
For a PowerPad package, Theta JC (bot) is more relevant as the majority of the heat flows thru the PP and not the leads of the IC.
Regards,
Ryan
Is there a reason we don't have Theta JC (Bot) in the datasheet in that case? Is that something we test in qualifications?