This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
given that the DRV8837 doesn't have internal clamping diodes, for a motor or solenoid application, these will need to be added externally, correct? If so, do you have a similar device that has the clamping diodes integrated or will the DRV8837 with external diodes be a smaller solution?
Thanks!
Hello Rick,
Thank you for reaching out! The short answer is "no" you don't need to add external diodes. But to confirm, can you explain what these external diodes are for?
Thank you,
Audrey
Hi Rick,
given that the DRV8837 doesn't have internal clamping diodes, for a motor or solenoid application, these will need to be added externally, correct?
It should drive DC motor or solenoid without additional clamping diodes. When driving solenoid with half bridge, the top and lower FETs are working in synchronous so when top FET turned off, the lower FET turned on to conduct the inductive recirculation current in the solenoid.
Brian