This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. Can I use protection diodes in the upper transistors for charging my Super-Cap. By connecting the battery to OUT1 and OUT2 (in 2-3 seconds)? (see my attached diagram)
2. If yes, Imax of the diodes in the forward direction?
3. Can I damage the circuit with this setup (lifetime)?
Notes: when I have charge the Super-cap, will I disconnect the battery and supply the device normal.
Resistor after the Battery = 0 ohm