Other Parts Discussed in Thread: MCT8329A, , DRV8300-Q1, DRV8343-Q1, DRV8350, DRV8300, DRV8328, DRV8320
Any suggestions to protect this IC from an automotive load dump (58V for 600ms)? The datasheet states 40V absolute max. Nothing about high voltage transients like load dump.
My motor needs to run continuously up to 32V….
Was planning to use two TVS diodes with a current limiting resistor between them but I cannot since the integrated FETS share the same input power at the IC (the motor will be using all 8A peak which will not allow the resistor).
I have not found a single TVS diode that will clamp at 40V and not breakdown below 32V…. that will handle a pulse of this length.
Any other ideas? Or am I stuck with an expensive cut-off circuit with multiple FETS and diodes and misc. resistors? This could defeat the purpose of using an integrated driver IC to reduce cost….