Hi,
We would to to use the DRV8231 to drive a brushed DC motor.
We need to be able to detect when the motor gets jammed (can't turn) so that the operator can be notified. The motor needs to cut out at about 1.7A.
The feedback from the driver passes through an opamp and is input to our microcontroller ADC. We can then take action. Our microcontroller ADC can handle 0-5V and 40mA max.
We've also added to LEDs which turn on when the motor turns on - a green LED for one direction and blue for reverse direction.
Referring to page 18 of the DRV8231 datasheet, please see attached image.
Does this look ok for our application?
Also, do we need to add a 600mOhm shunt resistor and if yes, in parallel with Rsense?
Appreciate any help.
Thanks