This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULC1001-DRV290XEVM: Demonstrating ultrasonic lens cleaning using the ULC1001-DRV-FL-EVM

Guru 10395 points
Part Number: ULC1001-DRV290XEVM

Hi, 

We are considering demonstrating ultrasonic lens cleaning using the ULC1001-DRV-FL-EVM. The ULC1001-DRV-FL-EVM product page states:

ーー
The ULC1001-DRV-FL-EVM is a bundle of the ULC1001-DRV290XEVM and our 20-mm diameter flat lens cover system (LCS) that can be used together to demonstrate ultrasonic lens cleaning.
ーー

Q1.
Does the LCS that comes with the EVM include all of the images below?

Q2.
If a customer manufactures using ULC, is it normal for LCS to be self-made because LCS is open source?
Or will some third party provide LCS?

Q3.
For the demonstration of ultrasonic lens cleaning, we are considering displaying camera images on a PC, etc. via USB.
My ideal is the demonstration below.
https://www.youtube.com/watch?v=zJQokIKyCrk&ab_channel=TexasInstruments
Could you please advise what steps I need to take after purchasing the ULC1001-DRV-FL-EVM?

We are a TI direct distributor. I can also email the ULC team directly if you are not comfortable answering using this form.
We look forward to working with the ULC team to bring this solution to market!

Thanks,

Conor