This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Daniel,
Someone from our team will be reaching out to you shortly to answer your questions.
Regards,
Pablo Armet
Hello Daniel,
In order to get a better understanding of your situation, I have some quick questions to ask:
Is your original question paired with the assumption that the same amount of power dissipation can be kept by decreasing the voltage from 24V to 12V and increasing the maximum drive current from 1.6A to 3.2A?
Or is the situation that you would like to have a lower thermal dissipation for a higher current (3.2A compared to the 1.6A in the datasheet for DRV8824)?
Regards,
Jaya Hari
The datasheet shows 1.6-A Maximum Drive Current at 24 V and TA = 25°C.
If we use the VM is 12V, does it mean we can drive it reach 3.2A?
Hi,
The 1.6A max output limit is due to the thermal limitation of the internal H-bridge FET, P=i^2 * R, where R is the FET on resistance, and not due to P=V * I. So even of VM is 12v the same 1.6A max is applied.
Brian
Thanks for your reply. I want to increase the maximum drive current from 1.6A to 3.2A on VM 12V situation.
1.6A is continuous output current, and it will trigger the OCP if the current is 1.8A or higher; therefore, 3.2A is a wishful unrealistic dream.
Brian
Daniel,
Our highest power stepper motor driver is the DRV8424 which has a min OCP of 4A. This would technically meet your specification.
Full scale current is still thermally limited to 2.5A. If you need full scale current of 3.2A, you will need to consider a gate driver like the DRV8711 with external FETs.
Regards,
Ryan