Other Parts Discussed in Thread: DRV8830
Hello,
I want to use this motor driver to drive my 4 Peltiers (rated 5V @ 1,5A)
Can I use the DRV8908 in Parallel mode (i.e 2OUT to drive 1 Peltier) to drive my Peltier at 75% continuous without the device going into thermal shutdown?
Or should I use the DRV8912 (i.e 3OUT to drive 1 Peltier)?
Or, can you recommend some appropriate part please. We are really flexible, for example, 4 pieces of DRV8830 can also work?
We don't have PWM output from our MCU so something with SPI controlled and Internal PWM is required.
Thank you very much in advance.