This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8320: leakage issue

Part Number: DRV8320

Hi Team,

The motor has leakage problems, with very large spurs at the drive end and erratic spurs, causing the motor to spin abnormally.

(The Chinese in above figure is, "PCB copper thickness is 1 oz., temperature rise is 20 degrees, bus outer wire is wider than 149 mils, drain of MOSFET should increase copper area as much as possible to increase the heat dissipation of the MOSFET. The DRV8320HRTV uses GND copper to spread the heat. ")

Could you help check is there anything need to be modified? Thanks.

Best Regards,

Cherry