Hello, with Rosc = ~160k an audible hissing noise can be heard, replacing Rosc with a ~64k, the hissing noise is minimized.
With Rosc set to 64K, what are the ramifications? Does the Higher Osc frequency result in a fixed PWM?
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, with Rosc = ~160k an audible hissing noise can be heard, replacing Rosc with a ~64k, the hissing noise is minimized.
With Rosc set to 64K, what are the ramifications? Does the Higher Osc frequency result in a fixed PWM?
thanks
Hi Allen,
When using the Rosc = 160k the pwm frequency is 25 kHz. This is above the audible range of 20 kHz so you should not be able to hear pwm signal. It is likely that the hissing is coming from another source. There are multiple free frequency apps such as Sonic Tools that will assist in determining the location and range of hissing noise.
Best,
David
Hello David.
it's related to the DUT and is somewhat migrated by changing Rosc to 64K. What are the ramifications of selecting a Rosc below 160K?
this thread has a similar issue,
it's unclear how it was resolved.
Hi Allen,
TI does not recommend operating devices outside of specified parameters as it can lead to damaging the device.
The fPWM may appear to be slower at the output (causing noise), if the VSENSE pin exceeds VREF to often.
Using ROSC = 160k, try changing RSENSE to keep VSENSE lower than VREF.
Best,
David