Hi
we can only turn on the motor once and then turn it off. Under normal circumstances, the motor cannot be used, and the fault alarm will be generated. However, the abnormal part cannot be used directly, and it cannot be read when connected to the computer.
The problem is: there is no fault state and alarm, and then can not control the switch, this problem is not always, or the communication will not be connected to the board and the gui communication, very unstable
Could you please help confirm the cause
Thank you
The above is the test video of the defective product
Above is a good product test video