Hi, I need a 4-channel integrated constant current control IC with 40V voltage and 2A current or external FET. Can you recommend some models?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I need a 4-channel integrated constant current control IC with 40V voltage and 2A current or external FET. Can you recommend some models?
Hi Yang,
TI offers a wide selection of integrated motor drivers for many applications.
Based on the specs given, the following link is to our portfolio of integrated BDC motor drivers, filtered by:
2 or 4 H-Bridges
Vmax > 40V
Peak output current > 2A
Brushed DC Motor Drivers: https://www.ti.com/motor-drivers/brushed-dc-bdc-drivers/products.html#248=2%3B46&2122=2%3B4&2716max=40.01%3B50&sort=248;asc&
The DRV8714-Q1 is another option if a Gate Driver with external FETs is required. The DRV8714-Q1 is an automotive 40V, four channel half-bridge smart gate driver with inline current sensing.
Gate Driver (DRV8714-Q1): https://www.ti.com/product/DRV8714-Q1
Best,
David
Hi Yang,
I believe you may be interested in our DRV8803 motor driver. It is a 60V, 2.3A, quad low-side driver with PWM control.
DRV8803: https://www.ti.com/product/DRV8803
Best,
David