Hi,
I just purchased and setup the DRV8711EVM board with the supplied stepper motor, and followed the manual instructions to get the stepper motor running. However whenever I would run the motor, it would only run for a few seconds before the motor would stop, the fault or stall LED would not light up, it would just stop. And if I read the faults from the basic menu it wouldn't show any faults. And if I tried to change any settings, or run the motor again, no response at all. It was as if it was disconnected, even though the status LED was still flashing and the "hardware connected" message was still showing. I had to power cycle everything, including the GUI to get it working again. After 3-4 times of doing this, I pressed start steps, the motor ran for a couple of seconds, then I pressed pause steps, the motor continued to run for a couple of seconds, then a big spark and smoke from the PCB. Upon inspection Q1 and R14 are fried. I don't understand what I could have done wrong? I had 24V DC supplied, the supplied stepper motor connected, and the preset configuration loaded supplied by TI.
Regards,
Nathan