This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8837: Driving VCC at minimum level 1.8V

Part Number: DRV8837

We are using DRV8837CDSGR in our Camera project to control the IR CUT Driver On/OFF. SoC Qualcomm QCM6490 is controlling it but the issue is SoC IO level is working on 1.8V only so is it safe to operate VCC of DRV8837CDSGR at 1.8V?

  • Hey Abhi,

    Yes, this should wor, though I would be worried about any voltage dip under load conditions if the voltage dropped below the undervoltage condition.  

    I recommend you consider the DRV8212 or DRV8212P - its minimum VM voltage is 1.65V, has higher current capability, and it is the same size or smaller than DRV8837 depending on the package you pick. 

    Best,

    Jacob