Hello,
I am using DRV8462 to control stepper motors DINGS 17E2115AB4-69SNSN-130.
The supply voltage is 24V. I use physical STEP and DIR pins and control other registers via SPI. The motors run with full step and automatic 1/32 microstep with frequency 300Hz. I use stand still power saving, automatic torque and stall detection.
My problem is moving with a single number of steps, such as 1-5 steps. When I move a higher number of steps, everything is fine, but doing 1-5 does not cause any movement. The screw only makes a vibration but returns to its original position. I check this by repeating taking single steps, waiting, taking single steps and so on.... Is there any way to make a single number of steps? Will increasing the maximum current in the ATQ help?