We are using DRV8876QPWPRQ1 full bridge driver to drive a brushed DC motor. The brush DC motor has 3 Ohm coild resistance and 13mH inductance. Also, the is also ring varisor across the motor terminal. I have attached the specs of the ring varistor.
We are driving bridge driver in PH/EN Control Mode. I got smother switching across the motor terminal However, the motor current has negative spike. I have atached the ssnapshot here with 55% PWm duty cycle and 20kHz switching. (Green- motor terminal voltage, Blue - Motor Current)
My question is there any issue with the bridge driver configuation? We do braking during off state cycle of the PWM. Let me know if you need any additional question.