Hello All,
Any guidance on this is appreciated.
I have used the H-bridge driver in the following configuration:
I use this to drive a latching valve with a 20ms pulse. Upon valve closing there seems to be a reverse emf on the VDD_SYS_3.3V in the form of kick back from the inductive load.
It was my impression this would be freewheeled with the built in diodes but its not the case.
Is the combination of VCC and VM potentially causing this issue OR I may be doing something thats not ideal when it comes to the driving signals IN1,IN2, nSLEEP?
Any thoughts are appreciated.
Thanks again,
Sasanka.