Other Parts Discussed in Thread: MCT8316A, MOTORSTUDIO
Dear TI Team,
I have a question regarding the compatibility of the MCT8329A with the motor studio GUI. As stated in this FAQ, the MotorStudio GUI currently only supports the MCF products of the MCx family, is there any plans to add support for the MCT products, specifically the MCT8329A? This question is born especially out of the fact that in my experience so far the GUI for the MCT8329A is more unreliable than for the MCT8316A and that ontop of that in the Motor Status section only the Algorithm State is displayed, the other values not being shown despite being read correctly via I2C out of the registers.
Another unrelated and minor issue is that during the guided tuning, in the external clock section the MCT8316A is mentioned instead of the MCT8329A once.
Kind regards,
Simon Calvini