Other Parts Discussed in Thread: MSP-EXP430FR2355, MCF8316A
Hi Team,
The customer has completed the implementation of I2C communication and is currently conducting register read/write tests.
I would like to inquire about the above.
1. According to the data sheet, ISD_CONFIG Register (Address = 80h) [Reset = 00000000h].
But, actually read the register value, it is "64738C20h". It seems like.. as it is an EVM board, the EEPROM has values set in advance.
So, I wonder whether the value of ISD_CONFIG Register is "64738C20h" or not.
2. I tried operating Mcf8316aevm according to the quick start guide, but no control signal is output. Are there any additional tasks that need to be performed other than what is explained in the guide?
3. Could you please share an example code file that reads/writes SPD_LOOP related values?
(Code file used when performing a demo test using MSP430 microcontrollers Launch pad (MSP-EXP430FR2355))
Thank you.