Other Parts Discussed in Thread: DRV8899-Q1
Hi
How to connect to 1-2 phases stepper motor ? motor spec as below. thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
How to connect to 1-2 phases stepper motor ? motor spec as below. thanks!
Hi PY,
The motor you shared with us is a unipolar stepper motor. This is a 5-wire type and does not work well with bipolar stepper drivers. The DRV8889-Q1 is a bipolar stepper driver. Do you need automotive qualified device for this motor?
Please refer to this application note, How to Drive Unipolar Stepper Motors with DRV8xxx https://www.ti.com/lit/an/sloa312/sloa312.pdf.
You can ignore pin-3 of this motor and leave it unconnected. Connect 1 and 5 to AOUT1 and AOUT2 and connect 2 and 4 to BOUT1 and BOUT2 of the DRV8889-Q1 or any other bipolar stepper driver. With this connection to the DRV8889-Q1 only full-step mode should be used. No other microstep mode will be supported.
Regards, Murugavel
Hi Murugavel,
Yes, Q-grade is needed. which device will you suggest to drive this motor? thanks!
Hi PY,
Please review the application note. Like I mentioned if you drive with DRV8899-Q1 (DRV8889-Q1 may be overkill) you can use only in full-step mode. EVM is available for evaluation.
Regards, Murugavel