Other Parts Discussed in Thread: DRV8214,
What is the accuracy and repeatability of position control in DRV8214/DRV8234? Are there any limitations – low current, stall, etc.?
I want to vary my supply voltage but maintain constant motor speed, how can I achieve this? Do you have any motor drivers that help with that? The motor needs to run at a constant speed even when the VM voltage varies from 14V to 8V. I would also like it to maintain speed even when a load is applied.