Hello Murugavel,
We are utilizing the CSA output analog voltage information, converting it to digital using the MCU ADC, and determining whether the current exceeds the set threshold or not.
Currently, we have configured a 25A current threshold through the internal ADC in the firmware. Below is the overcurrent waveform of the motor.
My question is, we have observed the motor current increasing up to 49A while we have set the threshold at 25A. Why is there an increase in current after the overcurrent triggers? Our client has been monitoring the logs, and they indicate that sometimes the maximum current increases up to 30A. Since we have set the threshold at 25A and the logs show higher currents, we need a clear explanation as to why the current is exceeding the set threshold.
Thanks,
Sonali