This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ULC1001-DRV290XEVM: Best way to connect multiple LCS together

Part Number: ULC1001-DRV290XEVM
Other Parts Discussed in Thread: ULC1001

Hello, is there a way to connect multiple LCS together (4 in my case) without needing too much additional circuitry? I only need 1 LCS to have sensing capabilities, the others can just follow, turn on/off. Thanks.  

  • Hello, 

    There needs to be one ULC system (ULC1001 + Driver) for each LCS. ULC1001's internal algorithms use IV sense data from the LCS that allow for overall operation and sensing capabilities. Any other connections added between ULC1001 and the LCS will significantly change this data. 

    Regards,
    Sydney Northcutt