UC2625-EP: Gate driver IC along with integrated MOSFETs for UC2625-EP

Part Number: UC2625-EP

Tool/software:

Hello,

We are using UC2625MDWREP as a commutation chip which generates gate pulses for High side and low side outputs for controlling three phase BLDC Motor. With UC2625MDWREP , max 20V motor can be directly connected , but we have a requirement of 400V.

Motor requirement is as follows:

Voltage - 400V

Current - 5A

Is there any gate driver IC along with integrated mosfets which takes the gate pulses from UC2625MDWREP to control the motor.