Tool/software:
Greetings,
I've run into an interesting issue with the DRV3946 driver.
We have an application that uses 4 of the drv3946's to drive 8 valves. The valves are close to each other (about 3mm) and when the wire to control the valve is run between the valves, disabling a valve will induce a PVDD_OV response on the valves adjacent to the valve that has been deactivated. We have rerouted the wires so that they are not running between valves and this has helped, a bit, but the error still occasionally occurs. I have tried to increase the PVDD_OV deglitch time to it's maximum value with no effect.
We have also installed a shortly. diode on the output to ground to try and control this spike, so far with no success.
Also, PVDD_OV warning always asserts due to our power supply supplying 24 volts for the valves and the threshold for lvdd_ov warning appears to be 20 volts.
Is there something I can do to mitigate this? I know I can disable the warning and the error with the control registers, but that seems like it would not be the best idea.
Any insight you can offer would be of help.
Thanks
Rick