Hello,
I'm trying to use an MSP-EXP430G2 Launchpad and DRV10983EVM-TB target board to program a DRV10975 chip. I opened the programming tool, sloc316, in CCS Version: 6.1.0.00104 and built successfully, but when I try to debug, I get the error: "MSP430: Error connecting to the target: Could not find device (or device not supported.)" I've tried a few different DRV10975 chips.
I was able to program the M430G2553 that came with the Launchpad with a sample code (blinking light) without issue.
Thanks,
Ben