This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8307 To prevent hunting motor

Other Parts Discussed in Thread: DRV8307EVM, DRV8307

Hi,

My cutomer is using DRV8307EVM with customer motor.
This motor is operated at EVM.
But motor is hunting, and speed can not be up even if PWM duty is up.
Please see the attached file.
This is waveform of U phase.

His motor characteristic and condition is below.
- Poles is 12 poles.
- Torque constant is 24 mN/m/A
- Motor indactance is 4 mH
- VM is 18V
- OC setting is default of EVM(5A).

What should we changing of DRV8307 setting to prevent hunting motor?

Best regards,
Shimizu

DRV8307.pptx