This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We need your advice for our PLC control unit that is used to operate several hydraulic solenoids.
Our case and requirements are as follows:
We have analog controlled solenoids that operate with (2 to 28 volts DC) & (0.3 to 2.5 amperes).
We need to control the above mentioned solenoids using analog PLC that gives output signal (0 to 10 Volts DC) or (4 to 20 milli ampere)
So we need a solenoid driver to operate our solenoids modulation using the PLC signal output.
We got your DRV8844 and we connected it as follows in a circuit:
After trying this setup didn’t give us our requirements.
We need to know if these connections are correct.
Also we need your advice if this any further components or additions needed for the setup to achieve our requirements.
Hi Rick
1- the output that we get is always 10 volts without even getting any signal from the plc ( always on)
2- we didn't use the EN1
3- the out put of the plc is a modulating output +ve signal with the -ve signal ( logic ground ) is from 0 to 10 volts ( but still this dont change the output of the driver under any condition.
4-the plc can give the following - from 0 to 10 VDC
- from -5 to 5 VDC
- from 0 to 5 VDC
- from 4 to 20 mamp
thank you for your support