1. How is the configuration of the different motor register parameters different?
2. What parameters are required to be configured when driving the motor?
3. When the motor is running, the wrong indicator is always flashing.
4. Is there any significant damage to the motor without error checking?
5. Is there a driver to refer to?