Hi team,
i will try to run a motor on low speed( 1 RPM ) to high(700 RPM ) speed, But it is not work in lower RPM means less than of 170 RPM,
It means, input step rate is more than 500 HZ with full step it works fine, but less than of step rate 500 HZ it is not work properly, i got a sound, motor is energized,
MOTOR specification is:
motor current = 0.72A (single winding)
Isens register = 0.2ohm
Vref set = 1.1v and sometime varied but it not works,
please give me solution,i will waiting for your reply....
Thanks in advance:)
Reagrds
Krishna