This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983: BLDC Ceiling Fan Controller with Sensor-less Sinusoidal Current Control, TIDA-00386 (Flyback Transformer Datasheet Discrepancy)

Part Number: DRV10983

Flyback Transformer Datasheet Discrepancy

Hello,

I am working on a BLDC motor driver using the DRV10983. In the application note it refers to a transformer that is used in the AC-DC to generate 24VDC from AC mains input. Here is the datasheet of the transformer.

http://www.ti.com/lit/ug/tidu354/tidu354.pdf

We are building that transformer right now but we have noticed a discrepancy between the bobbin datasheet and the photograph of the assembled transformer.

Please compare Page 2 and Page 3 in the datasheet.

Can someone please throw light on this or if there is a corrected datasheet that will help too.

Thanks and Regards

Ajay