Hi,
I need resolution on this as soon as possible. We are using the DRV8848 IC on one of our projects and it is showing a nFAULT when I powered the board without moving motor or anything else. I can move the motor (H-bridge) active but the Fault still persists. I have a pull-up externally on my board of 10KOhms to 3.3V and I should be seeing nFAULT to be high but it isn't. Is there a reason why this is being pulled low?
Thanks,
Marth