This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8873H-Q1EVM: About setting of GUI

Part Number: DRV8873H-Q1EVM


Hi,

Could you tell me about the setting of the GUI?

Q1. What is "Ramp Rate" to set?

Q2. It seems that only 3 items (53.2V / us, 2.6V / us, 13V / us) can be set for "Slew Rate".
Are the others settings described in the datasheet(34V/us, 18.3V/us, 7.9V/us) possible?



Best regards,
Yuto Sakai