This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8837: Lower suspend mode consumption

Part Number: DRV8837
Other Parts Discussed in Thread: DRV8838,

Hi,

Customer is considering to use DRV8837 or DRV8838 to achieve a lower current consumption during suspend mode when the chip is not functional (with no input from pin5/pin6.)  They can support two input as PWM or non-PWM input control, may I know if there's a difference of suspend mode consumption between these two chips?  Or you have a even better proposal other than these two chip to achieve a lower suspend mode consumption?

Thanks!

Antony