Hi,
I have the DRV8312EVM with cards C2000 and TMS but i need to control the DRV8312 with MSP430 MCU.
1 - Is there's a Card fit into the slot contain MSP430
2 - if there's another kit contain both DRV8312 and MSP430
if no hardware available, is there's a firmware can be uploaded to msp430 to drive DRV8312 to run BLDC sensorless.
Thanks