This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
The customer is experiencing below issue and needs your help.
In operation, the motor will suddenly go offline. View the status of DRV8711, it is a stall alarm. At the same time, faultn is equal to 0, and staln is equal to 0. If the direction of motor motion is rewritten, the motor can move normally. The circuit is boost circuit. The control method is to use the timer to do the flip of the IO port to generate a square wave.
Thanks.
Annie
Hi Annie,
I have a couple questions:
Hi Pablo,
Thanks for your support.
The customer did not give me any response. You are able to close this thread now. Once there is feedback, I will let you know.
Best Regards,
Annie