This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8308: detailed procedure to run BLDC with microcontroller

Part Number: DRV8308
Other Parts Discussed in Thread: DRV10987, DRV8320

Dear experts,

This might look like a stupid question but please give your time to help me asap.

I have a BLDC motor (24V - 100W) called nema23 with specs as below picture:

1/ Can DRV8308 work with this specific motor?

2/ If possible, please provide the detailed connections according to this motor (especially for Hall connection)

3/ I will use a microcontroller to control speed, pwm mode, direction and brake. What can I do to make this motor run. I mean the detail step by step such as setting up mandatory parameters, and through spi or what?

I have read through the datasheet of DRV8308 but could not conclude all needed steps to make the motor run. I need to finish my prototype asap then will run into mass production.

Thanks in advance,

Dientu28