This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8843: How to configure DRV8843 to drive Brushed DC Motor?

Part Number: DRV8843


Hi Expert,

I am using DRV8843 to drive brushed DC motor, but I am a newer to motor driver, I want to use fast decay mode, and need to control turn on/turn off and motor speed, can you help me solve below questions?

1.How to control the turn on and turn off od my brushed DC motor with DRV8843?

2.How to control brushed DC motor speed with DRV8843?

2.I want to configure as fast decay mode, but I find two ways, one is AIN1/BIN1 and AIN2/BIN2 pin, the other is DECAY pin,  are these two pin settings conflict with each other? I mean which pin should I use to configure fast decay mode, use DECAY or IN1+IN2? And how  to deal with the other?

Thank you!

Rachel

  • Hi Rachel,

    I am using DRV8843 to drive brushed DC motor, but I am a newer to motor driver, I want to use fast decay mode, and need to control turn on/turn off and motor speed, can you help me solve below questions?

    1.How to control the turn on and turn off od my brushed DC motor with DRV8843?

     


    Set one input low and PWM the other input. Please see Table 2 of the datasheet. For fast decay, you should switch between Forward PWM/ fast decay or Reverse PWM/fast decay.

     

    2.How to control brushed DC motor speed with DRV8843?


    The duty cycle is used to set the motor speed.  The higher the duty cycle, the faster the speed.

    2.I want to configure as fast decay mode, but I find two ways, one is AIN1/BIN1 and AIN2/BIN2 pin, the other is DECAY pin,  are these two pin settings conflict with each other? I mean which pin should I use to configure fast decay mode, use DECAY or IN1+IN2? And how  to deal with the other?


    The DECAY may conflict with each other during motor startup and stall.

    If  the DECAY pin is set to a current level that is higher than the startup or stall current, there should be no conflict.