Other Parts Discussed in Thread: DRV8873SEVM, DRV8873X-Q1EVM
1.When I was using DRV8873HEVM, I found that the motor was working, but the Fault pin light was on. What could be the cause of this, and what test should I do?
2. What is the frequency of EN/IN1 and can it be set? And what does Ramp Rate mean(in EVM software)?
3. I want to confirm whether Itrip cannot be set in DRV8873HEVM, but can be set in DRV8873SEVM, Is there any other way to set current limit on DRV8873HEVM?
4. As shown in the figure, can Rsense be set via software? I see Rsense=390 in the schematic. What is the effect of setting Rsense in the software?