Hi. team.
I connected an inductor between OUT1 and OUT2 and simulated it with PSpice, but a larger current than Itrip flows.
PMODE : PH/EN Control Mode
IMODE : Fixed Off Time
Itrip : 1A
Itrip setting is 1A, but the current(from out2 to out1) is about 1.8A.
1. Is this simulation result is correct? Would you tell me the problems about the design.
2. Why is it different from the current(from out2 to out1) and Itrip setting ?
Best Regards,DRV8874_Questions_2020.11.11.pdf